Hi Team,
There is -9V/2ns spike on SW during Vout short test. Please kindly help check if the spike is OK.
BRs
Given
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
There is -9V/2ns spike on SW during Vout short test. Please kindly help check if the spike is OK.
BRs
Given
Hello can you please share waveform and illustrate how the measurement is done on switch node?
The switch node measurement should be done with low inductance return.
Hi,
the waveform is as below.
after checking the measurement setting, the negative spike can be reduced to -7.5V/5ns. Is it OK ? Thanks.
BRs
Given
Is this at full load current?
Are you using tip and barrel method for probing switch?
This is wirebound device, I anticipate some ring. This amount of ring seems a little excessive (see fig 38 in D/S), Note, this looks like it was taken at 1A DC load. At 5A, the ring amplitude will be higher.
Also, can you share schematic and layout? I would like to look at input cap placement.