This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23756EVM: Remove C6, C7

Part Number: TPS23756EVM

Hi Sir,

My customer asked that when their system work on light load status, can or not remove the C6 and C7 at the same time?

If have any side effects, please advise. Thanks!

  • Hello Henry, 

    C6 & C7 are the input bulk capacitors. They are required by the IEEE802.3 standard, and the DCDC will not startup without them. 

    They can reduce it to 33uF at minimum. Thanks!

    If this post answers your question, please indicate so by marking this thread as resolved. Thank you.

     

    Regards, 

     

    Michael P.

    Applications Engineer

    Texas Instruments