Hi team,
My customer have the LED registers set up to show battery status whenever a pushbutton is used/pressed.
After disconnecting from the charger the LED”S will show battery status with solid LED’s and while charging the LED’s will blink.
I have noticed when the battery status (when not charging) is in the 0% - 20% range the first LED is not solid and blinks when the pushbutton is depressed. It is not consistent but usually occurs from 0-10% and then turns solid from 10-20%. Shouldn’t it always be solid if not charging?
Thanks,
Jacob