This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63060: Output short Protection

Part Number: TPS63060

Hi,

My customer is evaluating TPS63060.

The device is damaged by turning on(EN: L→H) on output short condition.

Is this correct behavior?

VIN=9V, VOUT=5.5V

Best Regards,

Kuramochi

  • Hi Kuramochi

    the device have short protection feature. so i think the IC shouldn't damage in the condition. not sure if the damage is caused by the special setup. could you apply an EVM for  reference. 

    also review the schematic and layout to check it they follow the suggestion in datasheet.