This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We encounter a supply shortage on TPS548A20 and consider replacing it with TPS549A20 which is with the PMBUS interface, besides some slight different default settings such as frequency and start-up time, the main problem is that the PMBUS pins will be grounded, will it be a problem if these two pins are not well pulled up?
Thanks ahead
-Sandy
The PMBus pins can be grounded and the device will use the default settings.