Good day. I have a problem with the training cycle.
After the first charge of the battery with 4 cells, my capacity is calculated,
but after a while when I put it on the discharge, all data is reset and the battery is discharged without controlling its capacity.
I have run several cycles on different controllers and all 3 are not working properly.
Please provide a more detailed algorithm for creating a new battery with new chemicals.
When you change the chemistry, nothing changes in the protection settings, so it should be whether it is a malfunction of the controller.
The settings of the protection thresholds do not change after the change of chemistry and other settings remain the basic factory.
With the basic settings, the battery worked correctly and went through the learning process.
also after charging the charging indication diodes do not turn off when the recharge threshold is triggered, but remain in the state of charge indication.
are switched off only at connection of loading, then the value of capacity is zeroed.
Please help.