Is the via on the far side of the TLV70728 on the TLV70728EVM-612 a tented via, or an un-tented via?
The user guide calls out a 6-mil via under the TLV70728. Is there any concern using a 7.9-mil (0.2mm) via under the regulator?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is the via on the far side of the TLV70728 on the TLV70728EVM-612 a tented via, or an un-tented via?
The user guide calls out a 6-mil via under the TLV70728. Is there any concern using a 7.9-mil (0.2mm) via under the regulator?
Hi Corey,
The via is un-tented.
I imported the gerbers into Altium and modified the via for 7.9 mils. The via will still fit inside the pad but the hole size is slightly larger. The biggest issue is solder flowing through the via and not making good contact with the thermal pad. The fab house can guide you on whether this would be an issue. My opinion is that 7.9 mils should be fine.
6 mil via in the center pad:
7.9 mil via in the center pad. You can barely notice a difference.
Thanks,
- Stephen