Hi TI-team
When my customer measured the LED PWM ON TIME, the result looked like the black line in the figure below.
LED:152Hz
PWM input:0.016%
LED Duty:0.016/65536/100=10 => 10/8192*100=0.122%
LED PWM ON TIME: 0.122/100/152=8.03us
The time is short when measured at 1/2 of the rise and fall.
Does this mean that the time is originally delayed for the rising edge of the red line?
Does this have any effect on the ”SLOPE_SELECT[2:0]” setting in ”8.3.6.3 Sloper” in the datasheet?
Best Regards,
Koji Hayashi