This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62130A: Switch node abnormal at light lodes

Part Number: TPS62130A


Hi Sirs,

The TPS62130A design spec is 

Vin: 3.3V;

Vout: 1.15V

I_load: 0.16A

Fsw: 1.25MHz 

Could you help check the switch node at light loads (0.16A), is it operating in power save mode? 

We measure the min switching level is -0.6V that under spec rating -0.3V, any impact?

Please help advised if any design mistake.

Thank you.

Amos.

I= 0.16A Loads waveform

@0.16A light Loads

I= 2A Loads waveform

@2A Loads

schematic

TPS62130A