Hi,
I would like to know if we can connect a 10K pull-up powered at 12V at the input of the TPS79333DBVRQ1 or TPS79333DBVRG4? The situation may happens when all my surrounding circuit is unpowered.
Since the current that can pass through the LDO's input or output would be limited by the 10K resistor, is-it still possible to damage the LDO itself (ABS max is below 6V for both in and out sides)?
Thanks,
Denis Alain, Eng.