This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: REG2

Part Number: BQ76952
Other Parts Discussed in Thread: TCAN1051
The BQ76952 datasheet shows an example application where the REG2 LDO output is supplying 5V power to a CAN transceiver.  However, the LDO output current limit of 45mA is too low to meet the supply current requirements of TI's TCAN1042 or TCAN1051 transceivers (80mA max in dominant mode, up to 180mA with the bus faulted).
Is there a recommended CAN transceiver which will not overload the REG2 output of the BQ76952?