This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2595: About the resistance value of the ILIM terminal

Part Number: TPS2595


I have a question about RLIM of the power load switch "TPS259541DSGT" with high-speed overvoltage protection.

Although the data sheet states that RLIM is Max 5000Ω (current range MAX 0.5A) Due to our mistake, we designed the circuit as 12000Ω (current range MAX 0.2A).

At this time, it seems that the overcurrent protection function is operating around 0.2A, What kind of trouble will occur?
Is there anything such as the current limiting accuracy cannot be maintained?

Please answer.