This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51219: Design calculation tool(power coils, capacitors(CCFL), and FETs)

Part Number: TPS51219


To the person in charge
Hello

My name is miyazaki
Using TPS51219, peripheral parts under the following conditions
I would like to select power coils, capacitors(CCFL), and FETs.
I want an auxiliary design calculation tool.
Please give me a draft of the circuit diagram.

Input voltage range: 8.0 to 15V (rated 12V)
Load current: 0 to 3.0A
Output set voltage: 1.0V ± 3%
Output ripple voltage: 30 mVp-p or less