Hi TI,
I have a buck converter during start up showing -6.6V at HS pin to COM pin. All traces is direct and short to reduce the parasitic inductance. However, there is still visible undershoot of around -4V across the bottom MOSFET D-S and HS pin to COM pin. In LM5106 datasheet, its allowable HS-COM undershoot is VDD - 15V = 12V - 15V = -3V only. Is it OK to proceed with undershoot more than 3V since we do not see any part damaged under such operating condition?
Regards,
KK