This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ35100: BQ35100 Current Calibration

Part Number: BQ35100
Other Parts Discussed in Thread: EV2400

Hi,

  I am using BQ35100 EVM, EV2400, and BQ STUDIO combo to test the BQ35100 device features. Battery ChemID is set to 0x608 (TADIRAN, LiSocl2,19AH).

 Also I am using two battery mode (J3 is set to 2-4s). Option-A register EXTVCELL bit is set. and I am applying 7.3V ( 2X3.6V) to BAT + and BAT- points.

It is reading Battery voltage accurately (BQ STUDIO ->Registers->Voltage) as 7.3V, but for current reading it is showing -16mA when 0mA is flowing between PACK+ and PACK- points.

I have calibrated the current reading by applying 50mA load between PACK+ and PACK- points, and so it read 50mA as -50mA, but 0mA current is showing as -16mA.

I am not really sure how to fix this issue, Please let me know how can I fix this.

Thanks,

Naga.