Part Number: BQ25302
BQ25302EVM uses 1 uH MAPM0420LA1R0M-LF inductor that is difficult to source. I'm working with the customer on alternatives, preferably physically smaller. If you have suggestions, they would appreciated.
For 2A charge current what would be the minimum inductor Isat requirement with margin? Can we get by with Isat = 4A? MAPM0420LA1R0M-LF has Isat = 8.7A typ.
ISAT ≥ ICHG + (1/2) IRIPPLE
Usually inductor ripple is designed in the range between 20% and 40% maximum charging current as a trade-off between inductor size and efficiency for a practical design.
Thanks,
Mark