This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65132: DELAY adjustment of model number without "S"

Part Number: TPS65132


Hi support team,

SLVSBM1H has the following description on page 22.

"DLYx Register - Address 0x02 (Only valid for TPS65132Sx)"

Isn't it possible to adjust DELAY with the TPS65132WRVCT without "S"?

Regards,
Dice-K

  • Hello,

    As the datasheet states, these register based delays are only available for TPS65132S. This version of the device (TPS65132S) has only one EN hardware signal that controls the enable/disable of both VPOS and VNEG rails where as other devices in this family have separate ENP/ENN controls for enabling/disabling VPOS and VNEG rails so their sequencing can be controlled externally with hardware signals. That is the main reason why TPS65132S provides these DLYx registers bits for sequencing.

    Kind Regards,

    Liaqat