This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28230: Full bridge topology question

Part Number: UCC28230

Hello team,

My customer is considering to use UCC28230.

Is it possible to use only O1_D and O2_D and then drive the MOSFET at opposite side in the bridge?

I mean it is just like full bridge topology with UC2825.

I think it is OK to configure UCC28230 full bridge with only O1_D and O2_D outputs up to 50% duty cycle.

Do you think I'm correct?

Regards,

Itoh