This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54362 DC-DC converter

I have used this TPS 54362 IC and configured it to withdraw 5V/2A and my input is 24V DC.

While testing the Evalution board and my designed PCB bot the output are get affected when we are placing a mobile (Cell Phone) 

phone near to the IC and its peripheral component. The cell phone is in calling mode.

we are observing about 2.3V deep in the output, some time the IC get reset as the my RST_th is set to 4.5V.

some time it match with the requirment of the reset and some time not.

can anybody give me what should be the precaustion should be taken to avoid this problem?