This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: 14S battery connection method?

Part Number: BQ76952
Other Parts Discussed in Thread: BQSTUDIO

Hello,TI experts.

I am designing a 14S battery,The connection is carried out in accordance with TI specifications, but I found that this connection method will cause the static power consumption of the cell 13 to increase.cell 13(8uA), cell 12(1.5uA), cell 11S(1.5uA)...

        bq76952-14S-2021-4-12

  • Hello, TI experts.
    I am designing a 14S battery, The connection is carried out in accordance with TI specifications, but I found that this connection method will cause the static power consumption of the cell 13 to increase. cell 13(8uA), cell 12(1.5uA), cell 11S(1.5uA)...


  •  In order to solve the problem of large difference in static power consumption between VC13, VC12, VC11...
     I connected VC14 and VC15 to VC16 and found that the static power consumption of VC13 has become 1.5uA, which is the same as VC12, which makes me excited.
    Excuse me, can I connect like this? Is it allowed to connect VC14, VC15 to VC16?
  • Hi JM,

    Table 16-3 in the device datasheet describes how to connect unused pins. For the VCx pins, there must be a battery cell connected on VC16-VC15, on VC2-VC1, and on VC1-VC0. All other VCx pins can be shorted as needed.

    So for this example, I suggest connecting VC13,VC14,VC15 together. 

    Best regards,

    Matt

  • Hi Matt,

    Do you mean that VC16&VC15, VC2&VC1,  VC1&VC0 must be short-circuited? 

    No matter what the number of strings? 

  • Hi JM,

    No, these are the pins that cannot be short-circuited. There must be a cell connected between VC15 and VC16. The same is true for VC1/VC0 and for VC2/VC1. 

    Any other inputs can be shorted to each other. 

    Matt

  • Hi Matt,

         I understand what you mean,  in order to average the power consumption,the schematic diagram VC12&VC13 is short-circuited, VC14&VC15 is short-circuited, and then is it possible to configure this on bqstudio?

        

        

         

  • Yes, this looks correct.

    Best regards,

    Matt