This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28951: UCC28951 Without output mosfets.

Part Number: UCC28951
Other Parts Discussed in Thread: UCC2895

Hello. I plan to do a Full-Bridge phase shift converter with ZVS. Output 340V @ 2A.

I would like to use the UCC28951 controller but the Texas development tool limits the output to 50V. I think it's because of the two output mosfets, in the figure below.

I would like to know if it is possible to use the controller in the topology of the Figure below: Only with the 4 input mosfets. With output of 340V 2A.