This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD19532Q5B: How to add to PSpice simulation model to Cadence 17.2

Part Number: CSD19532Q5B

Hi Team,

Our customer would like to incorporate CSD19532Q5B to Cadence 17.2 PSpice Simulation. He is requesting for instructions how to add to PSpice simulation model to Cadence 17.2.

Regards,

Danilo

  • Hi Danilo,

    Thanks for promoting TI FETs at your customer. The PSpice model (.LIB file) and schematic symbol.(OLB file) are included in the zip file available in the product folder on TI.com. The customer needs to download zip file from the product folder and extract and save the files contained in it. In the Capture CIS tool, select place part and then in the Libraries box on the right, select add new library and select the saved CSD19532Q5B.olb file. This will allow the symbol to placed into the schematic. The customer also needs to add the CSD19532Q5B.lib file to the simulation profile which can be found under the PSpice pull-down menu in Capture CIS. After selecting new simulation profile or edit simulation profile, click on the Configuration Files tab and then select Library. Browse to the CSD19532Q5B.lib file and add it to the design. TI also offers PSpice for TI for our customers (available for download on TI.com) and the CSD19532Q5B is included in the built-in library.

    Best Regards,

    John Wallace

    TI FET Applications

  • Hi John,

    Thank you very much for this information.

    Regards,

    Danilo