Part Number: LM5175
I am interested in using the LM5175 to drive GaN half bridges that have built-in high and low-side drivers (FBS-GAM02-P-C50). The maximum allowable voltage on the half-bridge control inputs is 5V, and I have a 5V supply on my board already. Is it acceptable to drive the LM5175 VCC pin with 5V, and not rely on the LDOs from the VIN and BIAS pins? (leave them unconnected) This would keep the output voltages on the LDRV and HDRV pins in the 0-5V range.
There is a second question, which relates to tying the High-side driver reference pins (SW1 and SW2) to ground. The FBS-GAM02-P-C50 already has a level shifter built into it, so the high-side outputs of the LM5175 do not need to be tied to the switching nodes for generating the proper gate voltages. Is it okay to tie the SW1 and SW2 pins on the LM5175 to ground, or are those pins used for some type of sensing/control other than level shifting the high-side driver outputs?
Thanks,
Paul