Hi team,
Could you tell the division of x-axis of Figure 23 on the datasheet?
Could you also give some comments on the followings if possible?
- In figure 23, the input voltage transient is about 1V and the transient of Vout is about 5mV. So is it OK in general to guess if the input voltage transient is about 5V, the transient of Vout can be also 5 times, that is 25mV?
- If the input voltage transients more rapidly, the transient of Vout would be larger. Are there ways to guess the relation between the input transient time and the transient of Vout?
Regards,
Noriyuki Takahashi