Hi,
Excuse me, if my LP87702 does not require 5V boot function,
Can I remove L4 in the picture below? Is there any signal of PG0, PG1, GPO0 that I should remove too?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Excuse me, if my LP87702 does not require 5V boot function,
Can I remove L4 in the picture below? Is there any signal of PG0, PG1, GPO0 that I should remove too?

Hi,
If the boost is not functioning properly the device can create powergood faults to PG pins and/or interrupts depending on the used OTP. The device used (LP87702D-Q1) in the picture will create powergood fault to PG1 pin for the boost.
Boost will still try to switch even if the inductor is removed. I do not see why this would not work but this is not a supported feature by the device and not recommended by TI.
Best regards,
Samuli Piispanen