Part Number: BQ21061
can we use BQ21061 instead
, IN present design the ADCIN pin is not be used.
Are there any potential risks for battery charge or discharge is different voltage , like low voltage(2.5V/2.6V/2.7V).
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ21061
can we use BQ21061 instead
, IN present design the ADCIN pin is not be used.
Are there any potential risks for battery charge or discharge is different voltage , like low voltage(2.5V/2.6V/2.7V).
Hi Kevin,
The only differences between the BQ21061 is the ADC capabilities. This includes being able to read the charge current and battery voltage. Aside from that there are not differences.