This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5066IEVM-626:LM5066I Problems with the test

Part Number: LM5066IEVM-626
Other Parts Discussed in Thread: LM5066I

Hello,

I am testing the LM5066IEVM-626 evaluation board.

I have some problems:

I configure for ILimit = 1.5A and in the load they are passing 3A. But I don't see that it limits the current.

How can I tell if the LM5066I is broken? However, the telemetry data reading is correct and detects OC.

Can you help me with this?

Thanks.