This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54260: Schematic review

Part Number: TPS54260

Dear Team,

There is good new that we DIN the TPS54260 in customer's new project.

Could you help to review the schematic?

We appreciated your great support!

Many Thanks,

Jimmy

  • Hi Jimmy,

    Some suggestions:

    1. Place 0.1uF 100V cap close to VIN pin and D1 GND

    2. Add 0 ohm in series with C3

    3. pay attention on capacitance derating with 24V bias voltage, 

    4. C320 value should be around 100pF level, and DNP as first option

    5. need to simulate the circuit in Webench for proper COMP value.

    B R

    Andy