This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25601D: BQ25601D Excel Design Tool

Part Number: BQ25601D

Dear Sir/Ms.

Some Chargers will provide an Excel design tool. For example, to calculate NTC resistance. I can't find it on the TI website. Does BQ25601D have an Excel calculation tool that can be provided to customers?

Best Regards,

Kami Huang

  • Kami,

    For RT1 and RT2 calculation tool, please refer to http://www.ti.com/lit/zip/slurax7 and plug in the specified design information accordingly. Although it was developed for the BQ2589x, the principle is similar and can be used for BQ25601D with minor changes.

    Thanks,

    Ning.

  • Hello Ning,

    The customer wants to design Vth and Vtl, the calculation formula VREGN is to bring in 6V. But the customer actually took the BQ25601D evb to measure the VREGN voltage
    ① VBUS voltage is 5.0V~6.16V, VREGN voltage is VREG 4.99~6.159V,
    ② VBUS 6.17V~~6.35V, VREGN is fixed at 6.17V,
    ③ VBUS>6.35V VREGN has no output
    So this VREGN output seems to be different from the datasheet.
    I want to confirm it. Isn't Jumpber set?
    How to design the voltage divider resistor next to the NTC?

    Best Regards,

    Kami Huang

  • Hello Kami,

    The RT1 and RT2 values do not depend on VREGN since it is a percentage of VREGN used for the thermal thresholds. You should still see a voltage on VREGN when VBUS is over 6.35V. What is VREGN when VBUS is 9V? How much current are you drawing from VREGN?

    Sincerely,

    Wyatt Keller