This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24040: Charger control solution with multiple temperature conditions

Part Number: BQ24040
Other Parts Discussed in Thread: BQ21061

Hello all,

My customer utilizes BQ24040 as the charger solution.

However, the control condition is tougher than before. The condition depends on temperature is now shown below:

(a) above 40 degree : disabled

(b) from 10 to 40 degree : fast-charged (1C, larger than 500mA)

(c) from 0 to 10 degree : slow-charged (0.2C under 100mA)

This may require the software control as the solution. (Ex: I2C interface to MCU)

I wanna to ask if there is the suitable solution.

Thanks for the help!

Dave Chang