Could you please let me know what is the current sense comparator offset error? Also, what is the minimum VIADJ voltage that can be used for proper operation? The datasheet mentions that 0.5V results in 50mV current sense voltage , which would lead to erroneous operation.
Is this limit applicable only if analog dimming function is used or for normal operation of setting the output current as well (if PWM dimming is used or dimming is not used)?
Also, please explain how to set the fsw value for a design.