This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61022: About the operation when the LED is connected to the load

Part Number: TPS61022
Other Parts Discussed in Thread: TPS61087

Dear TI Team

I'm wondering if the TPS61022 can be used like an LED driver.

In TPS61087, which is also a step-up DCDC, there is a circuit example when the LED is used as a load as shown in the figure below.

Is it possible to load LEDs with TPS61022 with the above circuit example configuration?

Best Regards,
Y.Ottey