This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63060: About Electrical characteristics of the entire temperature range condition

Part Number: TPS63060
Other Parts Discussed in Thread: TPS63070

Hi,

The following contents are described in the electrical characteristics of TPS63060.



However, customers want properties over the entire temperature range.
New devices such as the TPS63070 specify electrical characteristics over the entire temperature range.



・Is there any information that defines the Min Max value and FB accuracy of the electrical characteristics of TPS63060?
・Is there any reason why the TPS63060 is only testing "TA = 25"?

Best regards
Yusuke