Hi Team,
There are two dimming modes in the 8863 data sheet. Is pure PWM dimming (8863) equivalent to Phase-shift or Direct PWM mode in 8866?

Also about the PWM Input in the picture below:

If BRT_MODE is set to 2h, can customer ignore the PWM Input?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
There are two dimming modes in the 8863 data sheet. Is pure PWM dimming (8863) equivalent to Phase-shift or Direct PWM mode in 8866?

Also about the PWM Input in the picture below:

If BRT_MODE is set to 2h, can customer ignore the PWM Input?

Hi Kygo,
It is equivalent to the phase shift dimming. not the direct dimming mode.