Hi all:
I am looking for a (3channel or single) indicator LED driver (Vf = 1.4V If= 10mA maximum). The control interface is 1.8V GPIO from MCU. But I can't drive the LED by GPIO directly. (the GPIO current fan out ability is not enough). I need LED's behavior is following GPIO High/Low (Turn on when GPIO is high). I don't need the memory function in LED driver. Is LP5522 suitable for my application ??
Could anyone help me with this case ?