Hi TI,
This is Darshan from Intel.
The mosfet package CSD87352Q5D is made of 7 Level and most of the simulation tools support only till Mosfet level 3.
Is their any equivalent model of CSD87352Q5D which is of Level 3?
If no, then is there any kind of S-parameter(s*p) file for the same given mosfet CSD87352Q5D.
either one is very critical for us.
Thanks,
Darshan G
Intel