This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25200-Q1: Wrong datasheet parameter?

Part Number: TPS25200-Q1
Other Parts Discussed in Thread: TPS25200

In the TPS25200 datasheet, the EN pin turn-on threshold(rising) is listed as 1.9V, whereas the falling threshold is listed as 0.6V. The total hysteresis is given as 330mV which doesn't make sense. Which of these parameters are wrong? and what is the right value?