Other Parts Discussed in Thread: UCC28950
Hi Expert
We are designing a 10kW CCM+PSFB CC&CV battery charger.
We are facing a problem that we can`t get full output.
Because of the hardware design ,we are not able to measure the transformer current.
But we can probe the voltage of transformer voltage instead.
In 100khz Fsw condition We can only output about 3kW even dutycycle is almost 100%.
Also ZVS is quite easy to achieve when the power is at low.(about 2%)
We did not use shim inductor.All resonant tank is rely on transformer leak inductance.
We think what cause this problem is we got too large leak inductance,and this make the available duty cycle be come small.
Since we can`t probe transformer current , for make sure what it is going on as we thought.
We try to reduce Fsw to 50kHz let current get enought time to able rise up.
And we are be able raise output power to 8kW at 100% dutycycle.
Before we going to redesigned transformer to reduce the leak inductance.
We just want to check how you think of it.