This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51551: Instability and short pulses

Part Number: LM51551
Other Parts Discussed in Thread: LM51561

Hi, 

By mistake I clicked “Resolved” in the forum without having had a proper technical discussion with TI. My question is therefore re-posted here.

We use your LM51551DSST in an isolated flyback DC-DC converter with optocoupled feedback into the COMP pin. With no other load than the feedback system or a 1k static load resistor the regulator is able to provide the correct DC output voltage. However, there are stability issues as the power load increased. At present I can pull some 10W out of it. Go above that and it shuts down.

Input voltage: 5VDC. Output: 13-15W into 50VDC.

The circuit uses a custom transformer with turns radio 12.3:1, primary inductance 5.9µH and saturation current 13A. 

Q: What are the known causes for the LM51551DSST to produce very short pulses on the GATE pin? This question baffles us and we can't debug the rest of the design while it remains.

In our design the clock frequency is set close to 250kHz. At that rate there is a rising edge on the GATE pin. A great number of the pulses are very short (200ns). We have two previous revisions, one that displays short pulses, another one that never does. We have yet to tell the engineering difference that cause stability in one, not the two other ones.

As load current increases (using RND 320-KEL 103 300W programmable DC load), the -broad- pulses in my plot widen. The narrow ones have the same width, although they are somewhat rarer. Eventually, with increasing load, broad pulses grow so wide that the become united with the next narrow pulse. At this stage the regulator goes out of regulation, the output voltage drops and occasionally jumps up a little. By reducing the load close to 0W the circuit will start up again. The input voltage is not greatly affected by these mode changes.

With increased load I would instead expect the narrow pulses to widen, not the wide ones.

We have considered the following as causes of narrow pulses, and would greatly welcome your input since addressing the items on our list has not solved the issue:

  • GATE series resistance is too low (going from 10Ohm to 68Ohm brings improvement, not elimination of short pulses)
  • Improved decoupling of input and output (different decoupling show different behavior, not elimination)
  • Power-on with or without load (there have been brief runs of even-width pulses, they are hard to replicate)
  • LC filtering and series L (again, improvement not elimination)
  • Instability on CS pin (hard to distinguish due to ground lead pick-up, looks similar to GND measurement)
  • Feedback issues (COMP is DC with overlaid pulse noise pickup. It rises with increasing load power, from 1.5V@0W to 1.9V@10W)

We do use a spread-spectrum oscillator in this design, where the RT pin is modulated by a ramp function. This is to increase margins in EMC testing. Please note that the issue with the short pulses remains when we disable spread-spectrum oscillation.

Best regards, 

Børge

This is what GATE looks like on a scope plot.

  7178.StepUp_TI_pB01_20210415_sch.pdf

  • Hello Borge, 

    Now that we made sure that the transformer is properly oriented, I have few remarks to share with you: 

    1. I see that you are trying to synch the frequency externally, is this correct? What is the frequency of this oscillator? Does this problem persist if you are only using a 87k resistor on the RT pin? Anyway, you should make sure that the external frequency is higher than the one that you set with RH102.

    2. It looks like the converter does not really have enough bandwidth. Which cross over frequency did you select for your flyback? What happens if you try to increase the compensation resistor (RH106) ? 

    3. Can you add the scope plots of the COMP pin, RT pin and CS pin? 

    Kind regards, 

    Elisabetta 

  • Hello Borge, 

    Since I did not hear back from you, I will now close this thread. If you have further questions please feel free to post them here or open a new thread if this one has been locked due to time out. 

    Kind regards. 

  • We ended up using a different solution, so this is not relevant anymore. 

    The spread spectrum inside the LM51561 did improve matters, but it needed an additional spreader like the one in my schematic to modulate the voltage on the RT pin, not synchronize it. 

    Thanks,

    Børge