This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS542941: inductor selection

Guru 29720 points

Part Number: TPS542941

Hi Team,

The datasheet shows Recommended Component Values as the following.



My customer wants to use 3.3uH for L11 as substitute for 4.7uH under the following application.
-----------------------------------
Vin: 15V
Vout: 5V
Iout(max): 1.5A

R11: 124kΩ
R21: 22.1kΩ
Cff1: 10pF
C21: (22uF x 2) + (0.1uF)
-----------------------------------

Is it possible?

Best Regards,
Yaita