Other Parts Discussed in Thread: LM337, LM340, LM7800
Hi team,
Do we have upgrade device of LM317 (SOT223) / LM337 (SOT223)? Like device with better PSRR?
Thank you for your help!
Best regards,
Wendy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Wendy,
Below table shows a couple of options that have better PSRR.
| LM317 | LM337 | LM340 | LM7800 | |
| AEC Q100 | NO | NO | NO | NO |
| Output Options | Adjustable Output | Adjustable Output, Negative Output | Fixed Output | Fixed Output |
| Iout (Max) (A) | 1.5 | 1.5 | 1.5 | 1.5 |
| Vin (Max) (V) | 40 | -3 | 35 | 30 |
| Vin (Min) (V) | 3 | -40 | 7.5 | 7.5 |
| Vout (Max) (V) | 37 | -1.2 | 15 | 15 |
| Vout (Min) (V) | 1.25 | -37 | 5 | 5 |
| Fixed Output Options (V) | - | - | 5, 12, 15 | 5, 12, 15 |
| Enable | NO | NO | NO | NO |
| Power Good | NO | NO | NO | NO |
| Output Capacitor Type | Non-Ceramic | Non-Ceramic | Cap Free, Ceramic | Ceramic, Non-Ceramic |
| PSRR @ 100KHz (dB) | 38 | 19 | 50 | 48 |
| Noise (uVrms) | 38 | 1110 | 40 | 40 |
| Accuracy (%) | 5 | 2.4 | 2.5 | 3 |
| Vdo (Typ) (mV) | 2000 | 2000 | 2000 | 2000 |
| Iq (Typ) (mA) | 5 | 1.5 | 8 | 6 |
| Thermal Resistance θJA (°C/W) | 24 | 23 | 24 | 24 |
| Min Package Area (mm2) | 45.5 | 66.726 | 45.5 | 45.5 |
| Package Type | DDPAK/TO-263, SOT-223, TO-220, TO-220 | DDPAK/TO-263, TO-220, TO-252 | DDPAK/TO-263, SOT-223, TO-220, TO-220 | DDPAK/TO-263, SOT-223, TO-220 |
Regards,
Prakash L