Hi
TPS2549-Q1 in DCP mode, Apple charging certification failed.
The reason for the failure is that in the DCP mode, the charging information obtained by Apple is 2.4A. (is it because of divider3?)
MFI requires OCP to be at least 1.6 times greater than the nominal value of the charging current(2.4A*1.6=3.84A).
TPS2549-Q1 only supports a maximum of 3A, is there a way to make TPS2549-Q1 only get a charging current of 1.5A when the Apple device is in DCP mode.
best regard