This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25982: TPS259824 - About the TA data

Part Number: TPS25982

 I can't find the TA data at datasheet. Could you share the TA ambient temperature data as like below? Thanks

BR, Gary

  • Hi Gary,

    Device has a Junction-to-ambient thermal resistance. So as power dissipation across device increases junction temperature will rise above ambient temperature. In normal operation power dissipation will be some milliwatts and junction temperature will be almost equal to ambient temperature. So you can take ambient temperature range same as junction temperature range. Now during the fault conditions such as overcurrent, short at output when power dissipation across device increases then junction temperature can go beyond 125C and when it reaches 150C device will hit thermal shutdown . So you can say abs max junction temperature can go upto  150C.

    Regards

    Kunal Goel