I want to use BUCK1 for 5V (from 12V supply) and BUCK3 for 3V3, powered from BUCK1 since 12V supply is not possible.
BUCK2 is an independent rail...
So far so good, this works well on EVM when using the independent Enables.
Now i'd like the 3V3 track the 5V with the same ramp-up time (and one unique ENABLE)
I tried different configurations on the EVM with a resistor divider from 5V and with/without cap on the SS3 pin.
But the BUCK3 voltage always rises instantly without ramping up!?
Unfortunatelly the documentation won't help me any further, although it mentions in chapter 7.4.1.3:
Alternatively, one can use the soft-start pins as tracking inputs. In this case, connect the pins to the supply to be
tracked via a suitable divider network.
Can you please give some advise on adequate circuitry on SS3 and EN3 pins!?