Hi,
I do not understand the calculation of hardware protection.
After multiple testing, I wonder if there are no errors in formulas ?
I tried several values of gain, shunt and threshold, but the calculation does not correspond with reality.
The real test that I realized not correspond with the calculations.
Example,
Bq78pl114s12
Gain 5
Shunt 10mohm
HOCD 23.3A real, threshold value: 250, calculation : 30.6A
HSC 23.7A, real, threshold value 63 ,calculation : 31A
In addition, the Technical Reference Manual bq78pl114 of bq78pl116 and "What is a.tMap File?" do not have the same formula??
Help me, please?