This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5033: LM5033:Weak load capacity

Part Number: LM5033
Other Parts Discussed in Thread: TL431,

Design parameters:1、full-bridge circuit

                                2、Output Voltage:±190V

                                3、Output current:25A

During debugging, the no-load output voltage is normal. When the load reaches 3a, the output voltage is only 22V. 

The datasheet  indicates that the COMP voltage is between 1.5v-3.5, but when the voltage is within this range, the output voltage can not be stabilized and continues to rise.

So,The current comp voltage setting is 5V

What causes the above problems?