Other Parts Discussed in Thread: TPS63020, BQ25171EVM
Hello team. The question from customer. Thank you for support in advance.
We are going to use BQ25171 to charge a backup battery in our device.
There will be a situation, where main supply voltage is switched off, so Vin of BQ25171 is equal to 0V, and all of the system is supplied from Vbat.
So there are several questions on this:
1. While BQ25171_Vin = 0V, it results BQ25171 is supplied from Vout = Vbat = 2V4 – 4V5. Does BQ25171 contain a reverse current protection circuit? Is this mode allowable for BQ25171?We consider the situation when Vin = 0 may continue very long, till Vbat = 0.
2. What the amount of reverse current will flow into BQ25171, when Vout = 4V5?
3. Does BQ25171 contain a reverse battery protection?
4. To get the temperature value of battery, we want to measure the voltage on BQ25171_TS pin by ADC of external CPU. Can we connect TS pin directly to CPU_ADC input?What is the maximum voltage range of TS pin in the range of temp -40...+85C?