Hi,
i need to drive VREF to GND to reset the LM25066i slave address like described in the datasheet page 20:
"Reassigning or postponing the address capture is accomplished by holding the VREF pin to ground. Pulling the VREF pin low will also reset the logic and erase the volatile memory of the LM25066I/A. Once released, the VREF pin will charge up to its final value and the address will be latched into a volatile register once the voltage at the VREF exceeds 2.4V."
I want to use a reset controller for this job and it can hold LOW for 210ms long and drive a maximum current of 20 mA.
Will this be enough to drive the VREF low with 1uF capacitor? How much current can VREF drive?
Best regards,
Michael