This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need to be promoted a suitable power,many thanks

Other Parts Discussed in Thread: LM5155, LM5156

Dear:

Could you give me a suitable part number promotion ? 

parameter :24V input voltage transfer to +9V output and reverse 9V  output,  per channel meet 100mA current output,no need isolated chip。

  • Hello Cooper, 

    Thanks for reaching out. Do you need to have a positive and a negative output voltage rail at -9 V and +9V? If you are ok with a flyback topology, then you might want to consider a flyback/sepic/boost controller like the LM5155/LM5156 for example.

    Kind regards, 

    Elisabetta 

  • Hello, 

    Since I did not hear back from you, I will now close this thread. If you have further questions please feel free to post them here or open a new thread if this one has been locked due to time out. 

    Kind regards.