Part Number: UCC28881
Other Parts Discussed in Thread: UCC28910
Hello,
customer has following requirements:
Vin 40 -140VDC, Vout 12V, Iout: 500mA, non-iso (no use of transformator)
Can we use 2-3 UCC28881 in parallel? Other ideas?
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The UCC28881 devices were not design to operate in parallel. No one at TI has paralleled these devices as far as I know.
You might consider using the UCC28910 device setup in a high side buck instead. It should be able to easily handle the 500 mA output current.
Regards,